AXIS#.TUNING.QUICKTUNE.STATE

Description

Indicates the internal state of the most recent QuickTune process triggered by AXIS#.TUNING.QUICKTUNE.START.

Value Description Cause
-5  Set Tuning Error  Tuning parameters were calculated but could not be found in control loops installed on the drive. 
-4  Bandwidth Validation Error  Target Bandwidth could not be calculated and AXIS#.TUNING.USERBANDWIDTH was not set. 
-3  Inertia Start Error  Inertia measurement could not be started. 
-2  Inertia Calculation Error  Error in calculating load inertia. 
-1  Error  Unknown error occurred. 
0  Idle  QuickTune process has not been started. 
1  Measuring Inertia  Inertia measurement in progress. 
2  Validating Tuning  Tuning parameter calculation in progress. 
3  Done  QuickTune process completed successfully. 

Versions

Action Version Notes
Implemented 02-12-02-000 

-

General Information

Type Read Only
Units N/A
Range -5 to 3
Default Value N/A
Data Type Integer
See Also AXIS#.TUNING.QUICKTUNE.START
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.QUICKTUNE.STATE

5021h

06h

Unsigned8

-

-

Read only

No

AXIS2.TUNING.QUICKTUNE.STATE

5121h

06h

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5043

1

5043 (0x13b3)

AXIS1.TUNING.QUICKTUNE.STATE

Signed16

Read Only

Yes

70579

2

5043 (0x13b3)

AXIS2.TUNING.QUICKTUNE.STATE

Signed16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.TUNING.QUICKTUNE.STATE

5043

Signed16

Read Only

-